This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2HB50-Q1: Capacitive load inrush current control

Part Number: TPS2HB50-Q1

Hello there,

While using a capacitive load at the output of this IC it is taking a huge inrush current. The Vout slew rate seems to be fixed at 0.4 V/µs which is quite fast to control the inrush.

Is there any way to control the inrush current in a capacitive load ??

Thanks

Niki Sonowal