This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: LM74801-Q1

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM74800-Q1

Hi, 

we´re using the LM74801 in a common drain configuration. The Dgate MOSFET has 2,3mOhms only, and at currents app. lower than 5amps the reverse battery protection gets active due to (presumably) votage disturbance (EMI). Additional capacitance between pins A and C brings little improvement but will not eliminate the problem. Are there other measure I can take to achieve more robustness against EMI and to avoid unwanted switch off of the Dgate MOSFET?

Thank you help!!

Regards Thomas