We have a client that uses a lot uf bq24073 charge controllers in his application.
As this a linear controller, thermal considerations need to made.
Seveal hunderd units using this controller are returned with a burned up bq24073, despite its thermal protection features.
The PCB around the controller is charcoal black, so it must have been a quite high temperature.
I checked the schematic they did and it seems to have no errors. It is almost exactly as the application examples.
Ilim = 1.15A
Iset = 0.74A
TMR = 6.2h
Ub = 5V (USB AC Adapter Charger)
Battery = Standard LG 18650 Cell
Question:
What could lead to a complete destruction of the device, despite its thermal protection features?
A little suspicous for me is that, the TD pin is set to high -> Charge Termination is thus disabled.
This would mean, that the controller maintains the cell at 4.2V all the time, but still lets charing current flow?
This does not make sense IMHO.
Any insigts a greatly apreciated.