Other Parts Discussed in Thread: LM5116,
We have been working on a power supply design using the LM5116. This is a high temperature design so we are going to use the HT part. To save some cost (avoid destroying $300 parts), we put a LM5116MH on a DIP16 carrier board and have been swapping the two parts in and out as required for testing. We have a DIP16 socket on board to make this swap easier. For the most part this has worked well. We have two configuration of the board, one for 32V and one for 60V. The 32V design worked well with either of the part.
The 60V design has a bit of an issue. It works fine with the LM5116MH part, but when we swap in the LM5116-HT part (same board with no other changes) the board does not want to start up without a significant load on it. It seems to run fine with about a 300mA load, whereas if I use the LM5116MH part it will startup fine with just a very light load (~25mA).
Any suggestions?
Thanks
Ed H