Part Number: TPS1663
Other Parts Discussed in Thread: TPS2663
Hi Sir,
My customer is asking the TPS1663 if it can pass the ISO7637-2 Pulse 5b Load Dump test?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Henry
Is it acceptable if it is not AEC-Q100 qualified device?
Regards,
Rakesh
Hi Sir,
Yes, it is acceptable to use a non AEC-Q100 qualified device.
They also considered the TPS2663, is it available to use in the same condition?
What are the differences between TPS1663 and TPS2663 both devices? Does it refer to the different parameters shown in the comparison table?
Why did the TPS2663x develop two current limiting types of devices for 1x IOL and 2x IOL? Is it just for the pulse current support function on 2x IOL devices? what are the design requirements for the 2x IOL devices, if the customer needs to consider using them?
Hi Henry,
They also considered the TPS2663, is it available to use in the same condition?
Yes
What are the differences between TPS1663 and TPS2663 both devices? Does it refer to the different parameters shown in the comparison table?
The major difference is TPS2663 has B_GATE pin to drive external blocking FET to support reverse current and reverse voltage protection which are essential for surge protection. Rest all parameters are same
Why did the TPS2663x develop two current limiting types of devices for 1x IOL and 2x IOL? Is it just for the pulse current support function on 2x IOL devices? what are the design requirements for the 2x IOL devices, if the customer needs to consider using them?
We see some loads need higher pulsed current support in steady state to address their transient needs. Customer can decide based on the current profile of their load.
BR,
Rakesh