This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Firmware Version Mismatch

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: BQ34Z100-DEVICE-FW, BQSTUDIO

BQ ICs have been received with:

Firmware Version: 2.01 build 25

Auto Detect Device is 0100_2_01

I need the build 25 .bqz file but the BQ34z100-DEVICE-FW page only shows three available FW downloads.

Where can I get the build 25 FW?

  • Hi Lucas,

    When you download the most recent version of the FW and execute the file, there should be a .bqz file. Simple place this in the BQstudio config folder and it should now be available when you open BQstudio.

    Of the 3 FWs you circled the top is the R2 below that is the G1 and then the original FW.

    Regards,

    Evan