Hello expert,
I would like to know if we can use TPS53647 default code without programming and just use external hardware setting to set like current limit, frequency, Vout...etc. ? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
I would like to know if we can use TPS53647 default code without programming and just use external hardware setting to set like current limit, frequency, Vout...etc. ? Thanks a lot!
Best regards,
Ann Lien
Hi Ann,
I am not able to understand your question. What do you mean by using the default code without programming?
Thank you,
Dhanya Prem
Dhanya,
Do we need to pre-programming code for TPS53647? Or we can use default code on TPS53647 and set parameter from hardware setting? Could you consult with your team to know the default code meaning? Thanks!
Best regards,
Ann Lien
You can do both! If you already have a pre-programmed configuration file with all the parameters, you can load it into the Fusion GUI and run your device. You can also use the GUI to change the parameters you need. It is up to your preference on what you are trying to do.
Let me know if I interpreted your question correctly or not and I can re-iterate.
Dhanya Prem