Other Parts Discussed in Thread: BQ34Z100, BQ34Z100-R2
Hello,
I am updating my device (BQ34Z100-G1) FW from 0.16 to the new BQ34Z100-R2 FW (2.02) that is supposed to be compatible with all BQ34Z100 ICs. One issue I noticed is, that after updating, the voltage reading is drastically different.
Steps:
1. Default FW is 0.16, and I have the board calibrated
2. I program 2.02 to the IC and the memory in data flash is all reset
3. I use the same calibration data flash values (CC Gain, Voltage Divider, etc.) but now the voltage is drastically different than what is was
4. 2.02 has VoltScale, I check that even at '1' the voltage is drastically different than what it was on 0.16
5. I perform the calibration process (using the same CC Gain, CC Delta, CC Offset)
6. Voltage reading is now accurate, but Voltage Divider value in data flash updates itself from 9967 to ~33000
Is just updating VoltScale and Voltage Divider when moving to 2.02 the proper procedure for accurate voltage reading?