Other Parts Discussed in Thread: UCC27282


Hi,
I am using UCC27282QDRCTQ1 to drive the IAUT300N10S5N015 MOSFET for the motor controller application.
I have tested with 1kHz , 10kHz and 20kHz PWM from microcontroller to Hi and Li pin.
Without connecting MOSFET it's working fine like at LO pin I am getting 12V PWM and HO pin constant 12V high signal. However when I am connecting MOSFET IAUT300N10S5N015. LO PWM is OK at low side MOSFET of all three UVW phase and at HO 12V constant at high side MOSFET of U and V phase but for W phase high side I observed occsilaction at HO. Above test I done without connecting +Ve input voltage to inverter circuit only I have connected ground common with gate driver and microcontroller.
When I am connecting +Ve input voltage to inverter it's getting short with ground.
I have used 220nF bootstrap capacitors..I increased and tested with 4.7uF capacitor then occsilaction resolved but HO voltage increased upto to 17V-18V and when connected inverter +Ve input voltage it's getting short.
Please guide and support on his priority.