This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-C-PD-DUO-EVM: USB-C-PD-DUO-EVM

Part Number: USB-C-PD-DUO-EVM


Hi,

Can i connect USB-C-PD-DUO-EVM with PD controllers from other vendor.

I have already designed a PD controller based on reference from NVIDIA Orin.

The PD controller used in my design is PD3.0 compliant, so can i use USB-C-PD-DUO-EVM as a sink as 5V,9V,15V and 20V.

Any parameters i need to check before hooking up USB-C-PD-DUO-EVM with my design?

Thanks

Sanchit

  • Hi Sanchit,

    If by connect PD DUO EVM with other PD controllers, you mean a Type-C/PD connection using Type-C cable, then yes there should be no problem. The USB-C-PD-DUO-EVM should work with all PD sources and sinks out of the box.

    Best,

    Alex