Other Parts Discussed in Thread: TPS63810
Hello expert,
Do we have ABS max rating for Vin? We used TPS63810 for the front end and power 3.3V to TPS51200 VIN. But it seems like there is start-up spike up to 3.6V. We would like to know if you can provide ABS voltage rating for short term(within 20ns or one short period) so that we can know if this 3.6V is okay to use. Right now from datasheet, it shows 3.6V as ABS max. But we would like to know if TPS51200 can support that kind of spike during start-up. Thanks a lot!
Best regards,
Ann Lien