Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD97395Q4M: Gate-Treiber CSD97395Q4M

Part Number: CSD97395Q4M

Hello,

I have questions regarding the Gate-Treiber CSD97395Q4M, and I hope that you can answer these.

According to the datasheet, the recommended PWM should be 85%.

The measurements show a drop in performance only from 95%.

 

What PWM value can we increase up to?

Is it possible to use here PWM between 90-95%?

Is there a way to feed in an increased gate voltage from outside (extern) so that the bootstrap circuit is not necessary, and you can operate the Treiber up to 100% PWM?

 

I look forward to your answers

Thanks

Best regards

  • Hello,

    The boot capacitor is charging during off time. This is the reason that PWM duration should be less than 85% of the cycle time. 

    Increasing the gate voltage from outside can cause damage to the internal driver because the V_BOOT - V-BOOTR absolute max voltage is 6V.

    Regards