This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53688: IOUT_CAL_OFFSET setting is lost after power cycle

Part Number: TPS53688

Hi TI experts,

In my design i changed IOUT_CAL_OFFSET to have better current readout accuracy (to meet Intel VRTT requirements).

When i write offset values into registers and do "Write to HW" and "Store Config to NVM". After that, i powered cycle the board.

But after power cycled, the register value became the default value 0A.

Tried with Fusion 7.8.1, 7.9.3 and 7.10.1, all have similar issue.

Please help on this.

Thanks.