I was working through the example use-case in the datasheet to verify my own calculations.
I am a bit confused on the last section of 9.2.4.1, "For this particular application, the requirement is met as the result is 4.84 V."
Following the same values in the example, by using REN_TOP = 100k, REN_BOT = 15.5k, and VIHEN=4.5V. Based on the last line of the section mentioned above, I would expect to get 4.84V as the result of that formula, but I got 26.06V when I worked it out. I'm not sure if I'm just missing something or if I did the math wrong. Any guidance would be appreciated