Hello,
I want to control the system power using the Watchdog IC.
I haven't decided which Watchdog IC to use yet.
This is the block diagram of my project.

As I check, It would work properly after power on reset.
However, the reset level will be changed "Low(lower than Threshold voltage) to High(higher than Threshold voltage)".
It means that it can't turn power on after power is applied.
Do you recommend any solution to resolve this problem?
Thanks in advance.
Kevin