This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73: Connecting NC terminal to 3.3V out terminal does work?

Part Number: TPS73

Hi team,

When replacing TPS7333QDR with TPS77733DR, pin 7 changes from SENSE terminal to NC terminal. The SENSE terminal is connected to the OUT terminal, and they are both 3.3V on the board.

If it is replaced, pin 7 becomes NC terminal, so 3.3V will be connected to the NC terminal.

Is it OK to connect 3.3V (=OUT terminal) to the NC terminal? though I think it should be fine because NC terminal is simply not connected internally.

Your support is highly appreciated.