This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: Changing battery usage range to 80%

Part Number: BQ34Z100

Hi,

Based off cell specifications, recommended SOC window is 10%-90%.

I currently have a golden image that represents true SOC of the battery pack where SOC is 100% usable capacity for the user.

I need to set a usable SOC window smaller than 100% by limiting top end of charge to 90% and bottom end of discharge to 10%.

This setting would give the user 80% usable capacity for their application while displaying 100% SOC at 90% and 0% at 10% true capacity.

What configuration settings can I change to achieve this?

Thank you