Other Parts Discussed in Thread: TPS7B7702
Hello:
Regarding the TPS7B7702 chip, I have a question to ask
Can the EN2 SENSE2 LIM2 FB2 OUT2 pins of the chip be suspended when not in use, or what should be done
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
Regarding the TPS7B7702 chip, I have a question to ask
Can the EN2 SENSE2 LIM2 FB2 OUT2 pins of the chip be suspended when not in use, or what should be done
Hi Jimmy,
EN2 has an internal pull-down circuit, so channel 2 will be disabled if EN2 (and the other channel 2 pins) is left floating. If you do not plan to ever use channel 2, we recommend connecting all channel 2 pins to GND for improved thermal performance.
Regards,
Nick