Other Parts Discussed in Thread: UCD3138, UCD3138A, PMP21842, UCC25660
Hi TI Team,
I am going to design 3.3KW DC-DC power supply with following specification.
Pout - 3.3KW
Vout - 54V - 96V_dc
Iout max - 61A_dc
Vin - 390V - 410V_dc
Topology - FB_LLC with synchronous full wave rectification.
Kindly reply the following queries.
a. Can I use this UCC25640x IC in full bridge LLC also?
b. (if not) Please suggest appropriate IC for synchronous full-bridge LLC meeting above mentioned specification
c. Please provide the calculation sheet or design guide also.
Regards,