Part Number: LM2696
Hello,
Do you have any information on the Junction-to-Case thermal resistance figure for the LM2696MXA component please?
I have checked the datasheet but can only find the Junction-to-Ambient figure.
Kind regards,
Dan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2696
Hello,
Do you have any information on the Junction-to-Case thermal resistance figure for the LM2696MXA component please?
I have checked the datasheet but can only find the Junction-to-Ambient figure.
Kind regards,
Dan
Hello
As a very crude approximation, you can use a value of θJA = 38°C/W.
Please see the attached application note for more information about estimating
the thermal performance of your design.
Also, please follow all of the recommended PCB layout guidelines in the data sheet.
Thanks
Thanks for your reply.
Because of the HTSSOP package type (i,e. this component contains a large thermal pad to be soldered to the board) I was expecting a θJC figure much smaller than 38°C/W actually. I find sometimes this data may have been measured or calculated by manufacturers but not always included in the datasheets, I wonder if perhaps this data has been measured previously?
If any more accuracy for this component could be found, I would really appreciate it. I am running a thermal analysis model and this component is close to it's temperature limits.
Kind regards
Dan