Other Parts Discussed in Thread: LM25149
Hi Team,
I have a question about LM25149-Q1 dual phase operation.
Q. We use 2 units of LM25149-Q1 as single-output two-phase operation.
Can I ask how much IOUT difference of each phase(CH1,CH2)?
(for example, if 10A total output, the phase may shift up to 6A+4A, or 7A+3A...)
What factors determine the balance of the current?
Please tell me how it comes to balancing the current of each phase.
Thanks,