Hi,
This is a continuation of "Related Questions".
I'm considering using the LM5051 that was previously introduced to me. It is expected that the Vds of External-FET will be regulated to 45mV(Typ). In that case, the external-FET loss is expected to be 17W since it will handle a load current of about 19A. So is it okay to use one LM5051 + two FETs in parallel, or one LM5051 + one FET in two parallel circuits? Points to note in this case, which method is appropriate? Also if you have any other recommended configurations, please let me know.
Thanks,
Conor