Hi team,
In application where VIN=12V, VOUT=53.5V. And set the current limit according to formula below to 2.33A.
when both the input and output current exceed this overcurrent point, the phenomenon is that the output voltage decreases as the current increases, but it is still above 35V. Judging from the phenomenon, it seems that overcurrent is not triggered.
Does the setting of the overcurrent point not follow this formula? Or is the form of overcurrent protection not shutting down the MOS?