This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92638-Q1: Measurement of a resistor

Part Number: TPS92638-Q1

Hello , 

I have a measurement problem with one of your microchip : TPS92638QPWPRQ1

 

It’s used by one of our customers and the electrical schematic is  :

 

 

In our In Situ Tester (the card is not powered) we must measure the value of R4 (49.9 kOhms) but we can’t measure this because there is a parralel resistor on your microchip between pins 9 and 12 .

This value is around 4.5 kOhms but change at each microchip.

 

Can you tell me the value of this resistance and tolerances in your microchip or explain me how to check this resistance R4 ?

 

Thanks a lot.

 

Best Regards.