This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561: Inductor calculations for wide input range sepic converter

Part Number: LM51561
Other Parts Discussed in Thread: LM5156

I am currently designing a SEPIC converter with the LM51561 but am finding conflicting information online on how to calculate the required inductance of the coupled inductor. I have attached the calculations i've done so far but about the yellow marked parts i am not quite sure which one to use for the correct inductance value. The minimum and maximum input voltages are for two different power supplies, one is 12Vdc and one is 36Vdc. no in between voltages will be used. The output voltage of 27.5 is to eventually charge two 12V batteries in series.