Other Parts Discussed in Thread: UCC28C56EVM-066
I am currently working on designing a circuit for operating an LED strip, powered by a battery with a cutoff voltage of 55V and a maximum voltage of 150V. My goal is to step down the battery voltage to 48V, with a current requirement of 2.5A peak .
To achieve this, I have utilized the Webench tool and selected the UCC28C56H-Q1 as a suitable controller. However, I am encountering a challenge with the transformer part number. The information provided in both the EVM (Evaluation Module) and Webench is unclear.
Could you please suggest a specific transformer part number that is compatible with the UCC28C56H-Q1 for my application? Alternatively, if there's a better-suited option for my design, I am open to recommendations.
Your expertise and guidance on this matter would be greatly appreciated. Thank you in advance for your assistance.