This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Amuta,
Could you please share the footprint being used in your design? Below is the pitch measurement of the footprint of the model as well as the datasheet mechanical drawings. These are also the same footprint we used for our EVM.


Jesse
Hi Jesse,
Thanks for your reply but the measurements you shared is the pitch in Y -axis . I have issue with pitch in X - axis.
The pad centre to other pad centre gap is 1.6mm in land pattern , while in component mechanical drawing it is just 0.9 mm due to that more gap in pcb footprint the component leads not completely placed on pads.
Which will causing the dry solder on the component leads.
So kindly clarify is there any specific reason for giving more gap between pad to pad in land pattern? If anything please let me know.
Hi Amuta,
It is to account of pin width tolerance. This way it is guaranteed to have at least .35mm of pin on the of pad.
Jesse
Hi Jesse,
Still I am unable to understand the concept of giving that much gap between the pad in land pattern. Lead not soldered properly due to that and as per IPC 7351 component leads must be placed atleast 75% on the pad but here it lesser than that.
So it will not affect the performance? Please explain. Check below img. Blue outline is our actual component and yellow color is copper pad. It's very clear that component leads not sit completely on the pcb footprint.
Hi Amuta,


This is to account for the the pin tolerance of the device, for example, for pins 2-6, at absolute minimum, the pin length is going to be .4mm. This give a .05mm over hang from the pad and at 87.5% pin to pad contact. At maximum length .6mm, we are looking at 58% pin to pad contact, but on average you should be looking at ~75% pin to pad contact.
This should not affect the performance of the device. This is the same footprint that our other customer is using and we have not encountered any issues related to the footprint dimension.
Jesse
Hi Jesse,
Will it have any impact on the component performance if we customise the pad size according to the pin length of component?
Hi Amuta,
No, there should be no impact in performance if you customize the pad to be a little bigger. I just want to verify, at what length would you want to adjust the pad to?
Jesse