Hi team,
Is it ok to connect srp to Pack-, vice verca?
Regards,
Shoo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Shoo,
No, the Accumulated Capacity register should not decrease. So the register is increasing when the battery is discharging. Therefore, when the battery is charging the register should decrease. However, this gauge is to be used only with primary (non-rechargeable) batteries. Therefore, the battery should never be charged thus the Accumulated Capacity register should never decrease.
Sincerely,
Nick Richards
Hi Nick,
I mean if the small reverse current happen,
the Accumulated Capacity register would be decreasing ? bcz they are capaple of detecting charging current which means avg current register can have minus value.
My customer concern it might affect the measurement accuracy and it shouldn't have minus value.
Do you know the reason why this device can detect charging current? using same IP as rechargable battery?
regards,
Shoo.
Hello Shoo,
Yes, it uses the same IP as rechargeable batteries and yes, if there is a charge current then the register would decrease. However, if it is just very small reverse current for a short period of time then it would have a very minimum affect on measurement accuracy, which should not be a concern for a non-regular occurrence of reverse current.
Sincerely,
Nick Richards