Hi,
I hope you are doing well.
In order to deactivate the Safety PTC Thermistor, the BQ40Z50 battery pack manager datasheet states "to deactivate this feature connect a 10K Ohm resistor between PTC and VSS." In my schematic I have done so (please see image below) but I am unclear as to what needs to be done to PTCEN. Can this pin simply be connected to VSS as well? Does PTCEN still need to be connected to BAT? Any guidance you can provide would be appreciated. For my application VSS is connected to ground which is why I'm showing the connection to GND.
Best regards,
Joe DeWitt