Other Parts Discussed in Thread: TPS5450
Hi team,
I have a question here, if I give 30V input and the output is 15V, but the current of the rear end load is only 0.01A
According to the formula for calculating the inductance,Lmin=Vout*(Vin-Vout)/(Vin*Kind*Iout*Fsw),=15*15/(30*0.3*0.01*500000)=0.005
then Lmin=5000uH.
Would this be a problem if I had selected a 22uH inductance following a typical circuit on the data sheet?
Also, If I swap the connection between the output and the ground, will the output become -15V?In this situation, Vout*(Vin-Vout) will stay 30*(15-15) or be (-15)*(30+15)?