This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478Q-Q1: LM3478-q1

Part Number: LM3478Q-Q1
Other Parts Discussed in Thread: LM3478

Hello, good day. Our customer have a problem :

Does the lm3478 chip control the voltage loop and current loop together? For example,
in this picture, during normal operation, if the input voltage and output voltage remain unchanged,
will the load change current sampling voltage value limit the duty cycle?

The FB pin voltage is 0 and the current sampling voltage has not reached 0.325v. Will the IC continue to work in the current loop?

The feedback winding is short-circuited and the FB pin voltage is 0V, but the 3478 is still working (there is a driver output).
The problem is that the fb voltage is 0, why does it continue to work?
Channel 1 is the feedback winding voltage, channel 2 is the fb voltage, channel 3 is the drive, and channel 4 is the current sampling voltage.

Channel 1 is the feedback winding voltage, and channel 2 is the fb pin voltage. The picture above is the waveform of the feedback winding short circuit
  • Hi Yuhao,

    Thanks for using the e2e forum.
    LM3478 is a peak current mode controller, meaning it requires both the FB from the output voltage and the Isen from the current sensing to function properly.

    If the FB is pulled low, the device thinks the output voltage is too low, and will try to increase the output voltage until the overcurrent protection is triggered via the Isen pin.
    Triggering this protection will not turn off the device, but let it operate in a fault state where the driver signal will be turned off every cycle.
    This results in the behavior you observe in the waveform measurements.

    Best regards,
    Niklas