Other Parts Discussed in Thread: TPS61089, TPS61379-Q1, TPS61178, TPS61378-Q1
Hi Team,
in TPS61089 boost is stated when EN is low and VIN is present and above UVLO:
" Because of the body diode of the high-side rectifier FET, the input voltage goes through the body diode and appears at the VOUT pin at shutdown mode."
can you tell if it is the same with TPS61288L and/or TPS61178, TPS61379-Q1, TPS61378-Q1 ?
Do you maybe have a recommended boost that don't have this efect?
Vin= 5V, Vout=12V, Ioutmin= 0.5A
Best Regards,
d.