Hi TI
I have some questions about the Setting of TPS65994AD in the Application customization tool
1.Port1 settings-->Global System Configuration-->PP3 Config&PP4 Config
What does the two settings effect ? If I do not need the Sink Power, Can I disable the PP3&PP4
2.Port1 settings-->Port Configuration-->TypeC Support Options
What does this setting affect? And What does each option represent?
3.Port1 settings-->Transmit Sink Capabilities-->Number Valid PDOs
when I do not need Sink Function,Can i set to Zero
4.Port1 settings-->Display Port Configuration-->Multi Function Preferred
What does this option mean?Can I check it?