Other Parts Discussed in Thread: LMR16030,
Hi Team:
customer using LMR16030 / TPS54560BDDAR with 28Vin and 24V/3A use case.
at the beginning , the LMR16030 thermal performance works when test the short circuit test. but when work normal with 50W~40W load, the thermal is a little higher.
Then we decide to change to TPS54560BDDAR, The duty cycle during short circuit is 7.3%. meanwhile , we found the LMR16030 duty cycle during short circuit is 3%
do we have a solution how to reduce the duty cycle during short circuit from 7.3% to 3%?