Hello,
As we need to reduce the quiescent current of TPS55340 block, can we set the upper FB resistor 345K and the lower one 36K?
The input voltage(9V) of TPS55340 will always on when the product in sleep mode.
As a boost function group, there is a diode[D1 in reference schematic] connected from input to output. So the FB resistors are always powered by 8.5V.
The spec of I_fb is 1.6nA(Max 20nA).
So the combination of 345K/36K is a risk?
Thanks
Stephen