I'm developing a POE board and Input is 48V from the ethernet Jack. The board is a 4 layer board with the 2 middle layers being ground planes. I referenced this circuit on WebBench, but mistakenly changed CVCC to 1nF instead of 1uF. Now I measure 48V on the 48V TP pins 2, 3 both measure 48V after the CAPS charge. On pin 6 I have 2.5V and pin 7 2.8V. I don't think CVCC is my issue, but I'm new at this. I need help determining if that is my issue, if my layout is just wrong, or if something else is my issue.