Other Parts Discussed in Thread: LM70880, , LM5177
Hi TEAM
Our customers want the boards we develop to work well in 12V, 24V, and 48V vehicle battery environments.
At first, I tried to use a buck boost product (LM70880), but considering the cold crank test of the 12V system, I think I should use a buck-boost product.
So I think LM5118-Q1 is good for our development board. Is it right?
We need below specification for our development board.
Vin -> 4V~60V (12V, 24V or 48V)
: I think the Cold Crank test requires Min. 4V
Vout -> 10V (Max Current-> 6.5A, Normal Current-> 4.5A)
If LM5118-Q1 is not good, Can you recommend other product?
thank you.