Hi
The customer design with BQ7695202 (default output LDO1) According to the reference design, the circuit has a standby current of 10mA when powered on at 50V.
After disconnecting the 3.3V output of REG1, the standby current is close to 0mA.
The actual load current under test REG1 is 10mA at 3.3V. The input B+ B- power consumption is 10mA (50V). The NPN transistor generates heat.
NPN transistor model: FCX495TA
Please help check it.
Thanks
Star