Other Parts Discussed in Thread: TPS61021A, TPS61299
Hi team,
Our customer is looking for the device that is able to use below requirements:
Vin : 0.7V to 1.5V(AA battery)
Vout : 5V
Iout : 300mA
I search the device but there is no device much upper requirements. TLV61070A need 1.3V to start up, so when the battery voltage decrease under 1.3V, this device can't start up.
And in this requirements, input current is over 2A(TLV61070A's min current limit).
So I want to know if below using is possible by TLV61070A or TPS61021A?
Please some comment to below using or tell me other recommend device if you have.


Best regards,
teritama