Other Parts Discussed in Thread: LM5118, LM5177
Hi,
I am looking for a device or strategy which can suffice below requirement:
- Supply voltage: 12V/ 24V battery system
- Load dump voltage: 45V
- Cold-crank voltage: 2.8V to 3V
- Regulated output voltage: 3.3V
- Output current: 2A
Can LM5118 fulfil this? Is there another better solution or discrete design
Regards,
Prachi