Other Parts Discussed in Thread: BQ76942
Hi,
I am using the BQ76952 and looking at series vs. parallel FET configuration. Seems as if the data sheet and eval board use a serial configuration. My system will be discharging at 200A max and charging at about 35A. I can't seem to find any schematics or diagrams for parallel FETs or the pro's and con's of each configuration. Are there any white papers on this? Or is there a reference design with the FET's in parallel? If the FETS are in parallel mode, are the predischarge and precharge FETs used as well?
This also brings me to another question and that is how the discharge or charge current is detected. I understand it is via the sense resistor but I can't find a very detailed description of how the FET's are controlled when sensing the current.
Thanks!!
John