This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Thank you for using E2E,
I didn't find any P2P with MP1614, but the alternate solution is
TPS62827/7A (QFN), 4A |
TPS62865 (QFN), 4A |
Vin = 3.3V, Vout= 0.8V, Iout = 3A | |||
MP1614C | TPS62827A | TPS62865 | |
Inductor | 0.43uH | 0.43uH | 0.43uH |
Capacitor | 22uF | 22uF | 22uF |
Efficiency | 79.9% | 77.0% | 84.2% |
Power input (W) | 3.00 | 3.12 | 2.85 |
RThetaJA | 110 | 129.50 | 90.90 |
Thermal (°C) | 91 | 118 | 66 |
Package | SOT583 (2.1 x 1.6) | QFN(1.5 x 1.5) | QFN(1.5 x 2.5) |
Vout_ripple | 5.9mV | 1.7mV | 1.28mV |
L value used is 0.43uH with 17.6mohms DCR | |||
All values are based on Webench data and MPS simulator data. |
I will share you more information via email.
Thank you & regards,
Moheddin.