Part Number: TPS796
I am considering replacing TPS79633 with TLV75733. I have a question about the startup behavior of each device. Could you please confirm the following?
■TPS79633
1) When the input voltage rises, the output voltage becomes the same as the input voltage. Is this correct operation of the TPS796?
2) If it is correct, could you tell me why this operation occurs based on the internal structure?
■TPS79633 vs TLV75733
1) The rise behavior of the two devices appears to be the same. Is this correct?
2) If it is correct, could you tell me why this operation occurs based on the internal structure? If it is not correct, could you tell me why this operation occurs based on the internal structure?
Best Regards,
NIshie