This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: Output current issue

Part Number: TPS25947

Hi,

We are using TPS259470A version of the part in our design. In one of the boards, the load switch operation is not as expected. We have programmed the current limit around 1.5A minimum. Our input voltage is 3.3V. When we connect a load corresponding to 1.5A, the load switch output voltage is dropping down to 3V and output current is around 1.2A. We have conducted this test with external power supply as input source and set the current limit to 1.7A. This is not a design issue because this happens with only one board. We are not able to conclude whether the loadswitch IC is damaged or not.  We appreciate your inputs.

Regards,

Saravana