This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: IEC Certification for energy limited circuits acc. to IEC61010-1

Part Number: TPS1663

Hello,

with UL E-File E339631 the tests covers up a current up to 6.42A. Is there an IEC Certification in comparison to https://www.ti.com/lit/pdf/slvq011 with the high current? In the Certification for the IEC 62368-1 it's only been tested for 1.6A at 60Vdc.

I will use this component TPS16630 to create an ernergy limited circuit with 4.5A and 24Vdc.

Best regards,

Eric