Other Parts Discussed in Thread: TPS2121
I am currently trying to perform simulations using the TPS2116DRLR. The primary voltage is 3.3V and the secondary is 3V. I currently have the device set up in primary switchover mode where the device where the primary voltage will be the output until the primary voltage drops below PR1 threshold. In my current setup I have the PR1 threshold set up at 2.9 because the Output can not dip below 2.55V no matter what in this design. I know that when the primary drops out it takes a few microseconds for the secondary voltage to switch in. During that time, the voltage output will dip. I was hoping to prove in simulation that choosing a big enough output cap and a high enough PR1 threshold that I could minimalize that dip so that the voltage stays above 2.55V but I am not able to simulate the cross over in the simulation once the primary voltage drops out the output drops out and doesn’t switch over to the secondary voltage. Even if I don’t connect the primary voltage it never works off the secondary voltage please see graph below and set up below.