Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62840: power from 2x CR2032

Part Number: TPS62840

Hi,

The specs for the initial max voltage for CR2032 batteries indicate 3.4V. However, when starting draining current (i.e. 0.2mA)  the voltage starts dropping to a value close to it nominal 3V.
Is the TPS62840 (with input voltage up to 6.5V and absolute max 7V) suitable for designs using 2x CR2032 batteries in series?

Thank you for your support.