This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: Is there a maximum inductance?

Part Number: TLV62569


We are reusing the TLV62569 for multiple rails in the system. Of the rails we need to limit ripple current to <0.1A and minimize EMI.

The datasheet is focused around 2.2uH for the inductor, could we use 22uH instead? Any concerns with this?