This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8863EVM: Two questions about driving with an external power supply and SEPIC mode

Part Number: LP8863EVM


1. Is there a way to drive all the LEDs with an external power supply without using the boost feature at all? 

2. How do I facilitate the SEPIC mode which caps the maximum voltage at 24V? 

Many thanks, 

Genevieve 

  • Hi Genevieve,

    Our expert is currently celebrating Chinese  New Year and is out of office. He/she will reply to you after Feb.18 when he/she is back to office. Thanks for your understanding.

    Best Regards,

    Steven

  • Hi, customer

    1. Is there a way to drive all the LEDs with an external power supply without using the boost feature at all? 

    Yes, LP8863 can setup as a external power supply. see the datasheet description in below.

    2. How do I facilitate the SEPIC mode which caps the maximum voltage at 24V? 

    I cannot understand this question clearly.