Other Parts Discussed in Thread: USB2ANY
Hello,
Where can I download the USB2ANY_2.8.2.0_SDK_Setup.exe to use the USB2ANY with the BQ79616EVM?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Where can I download the USB2ANY_2.8.2.0_SDK_Setup.exe to use the USB2ANY with the BQ79616EVM?
You can download the "USB2ANY_2.8.2.0_SDK_Setup.exe" file here:
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/USB2ANY_5F00_2.8.2.0_5F00_SDK_5F00_Setup.exe
The SDK is not required if using a brand-new USB2ANY. If using a brand-new USB2ANY use the USB2ANY Firmware Loader instead and follow update set-up starting Step 5 in Section 1.1.3 Updating USB2ANY Firmware of the BQ79616 Graphical User Interface (GUI) User's Guide.